You are here: Tools > Softscope > Trace Zoom Feature

Trace Zoom Feature

The zoom feature is used to magnify or reduce a portion of a trace. Two zoom modes are available:

Time zoom

Used to expand/collapse the time-base in order to have a better view of the signal evolution through time.
This zoom operation updates the time-base value.

Amplitude zoom

Used to have a better view of a part of a signal.
This zoom operation updates the amplitude & zero offset value

The zoom operations can be done:

For more details on setting the amplitude, zero offset and time-base values, refer to Setting Scale.

Mouse Shortcuts

Action Result
Scrolling up the mouse wheel Expands the time-base value
Scrolling down the mouse wheel Collapses the time-base value
Pressing the Ctrl key while scrolling up Makes the amplitude value greater
Pressing the Ctrl key while scrolling down Makes the amplitude value smaller

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™